Water Treatment: Your Key to Greater Sustainability
Protect systems with pre-filtered process water
Obtained from rivers, lakes, wells, seas and the ground – water is used in industry as intake water in a vast range of processes. Careful treatment of the raw water via filtration is the key to efficient system operation. The treated water can be used as cooling water, membrane feed water, spray water or process water, for example. If the raw water is able to enter the system without being filtered, there are severe consequences. Avoidable consequences. Because automatic back-flushing filters, inline filters and screen basket filters can provide reliable assistance. How they should be used, and where, and what role mussels have to play in the whole scenario is all explained here!
Pre-Filtration is a Crucial Step in Water Treatment What filter do you really need?
Whether it's automatic back-flushing filters, inline filters or screen basket filters, use our filter check to find the right filter for your application. Because clean process water will benefit your entire system.
Make Process Circuits sustainable with Water Recycling This minimises both the consumption of fresh water and waste water discharge
Cooling Water
When cooling water is used, coatings often form on the heat transmission surfaces, which impair the transmission of heat and accelerate corrosion and abrasion. Deposits which accumulate over time can damage system components such as measuring devices and pipe fittings and the system can experience higher levels of pressure loss. All of this increases the maintenance workload and makes the system less cost-effective. To prevent this in fresh water and circulation water, our automatic, screen basket and inline filters are used for full flow filtration and offline filtration.
Process Water
Process water is used in production in many sectors of industry, for example as cooling water, washing water, boiler feed water or ultrapure water. The water collected from rivers, lakes, the sea or from the ground is initially loaded with particulate and dissolved material as well as microorganisms. This contamination needs to be carefully filtered out – our inline and back-flushing filters support you with your water treatment, improving your system's profitability.
Waste Water
In municipal and industrial wastewater treatment plants, valuable drinking water is often used for general cleaning and maintenance work. But it makes sense to treat the water coming from the secondary clarifier – as this avoids wasting drinking water. The discharge water is almost clear, in both dry and rainy weather, and contains very few suspended particles. This is not directly suitable for use as service water, however. Our water filters for the industry take care of the undissolved organic and inorganic substances that would clog the system.
Friedrich Wilhelm, Project Manager in Technical Sales at HYDAC Process Technology
While the types of particle contamination in processes are highly varied, the methods for removing them are just as diverse. Selecting the right one requires knowledge of the solid particle load and process data. A filtration goal also needs to be specified. No matter how much information and experience we have in separation technology, there are always new challenges that call for new technologies and solutions, as no two applications are ever the same.
Mussels Clog up Cooling Water Circuits How to fight mussel infestations with predictive filtration
In recent years, invasive mussel species have been spreading in fresh water, salt water and brackish water. Two of these species are in a class of their own – the zebra mussel (Dreissena polymorpha), and its sneaky relative, the quagga mussel (Dreissena rostriformis bugensis). While they are native to the Black Sea, they are unintentionally spread almost all over the world via ballast water and have now entered plants via natural water cycles. And more mussels means more problems in the systems. Cleaning infected systems is time-consuming, and often the entire system needs to be shut down.
Mussels and larvae are often killed off with chemicals (potassium chloride / hydrogen peroxide). Deadly for these sea-dwellers, but not entirely harmless in terms of materials, unwanted residue and health risks. In short, using chemicals does work, but this is extremely controversial, as well as costly. Taking preventive action is less expensive, and the costs are also more predictable. The key to success: filtration.
Protect your system – find the right process filter now
Great Protection against Small Invaders from the Sea Clean process water thanks to optimal water treatment
Coarse Protection for Vulnerable Systems
Our automatic back-flushing filter AutoFilt® RF3 takes care of large mussel bundles and some of the mussel larvae. It covers a continuous nominal flow rate of up to 7,500 m3/h. Flow passes through the wedge wire elements with a filtration rating of 50 µm from the inside to the outside during filtration. This provides your system with optimal protection from large collections of mussels.
Basket-based Protection against Mussel Larvae
To stop the mussels from spreading, the mussel larvae need to be filtered out of the system. The AutoFilt® RF14 series provides significantly higher filtration of mussel larvae. The self-cleaning basket filter has a finer filtration rating. With the standard filtration ratings of 20 µm and 40 µm, roughly 95% of mussel larvae are separated out.
Combination Solution with almost 100% Destruction of Mussel Larvae
A combination of automatic filters and UV disinfection kills off nearly all mussel larvae, as the microbes are destroyed in fractions of a second if the dose is sufficient. Our combination solution permanently reduces mussel infestations, system downtime, maintenance and excessive costs. No chemicals need to be used in the water filtration.
Our Solutions for Water Treatment
AutoFilt® Automatic Back-Flushing Filter
Our automatic back-flushing filters have been established on the market for many years – not least due to their high level of efficiency. There's only a one-time investment expenditure and no operating expenses. The self-cleaning function with our filters means that these maintenance visits are automatically eliminated, sparing you the costs for replacing elements and screens.
Inline Filters & Screen Basket Filters
Our inline and screen basket filters allow solid particles of all kinds to be removed effectively. A large variety of models and filter materials allows optimum adjustment to suit the particular filtration task and process conditions.
Your advantages
- Temperatures up to 400 °C
- Pressures up to 1000 bar
- High-quality filter materials made from Chemicron® metal fibre or wire mesh, and Processmicron® plastic fibre or glass fibre
- Filtration ratings from 1 µm absolute to 10000 µm
- Flow rates up to 3600 m3/h
- Skid/system solutions and special custom solutions
Skid Solutions and Custom Products
Whether it's managing high flow rates, combining coarse and fine filtration or using filters in conjunction with heat exchangers, we can supply custom system solutions. For optimal water filtration, we perfectly tailor the solutions to your needs.
Your advantages
- Filters and heat exchangers from a single source
- Custom design
- Perfect for retrofits in existing systems
Water Treatment in a Major Swiss Project: CirculagoPioneering for geothermal power generation & building technology
Heat exchangers and large heat pumps (water-water heat pumps) are often used in modern heat generation involving deep geothermal energy, lake energy and the use of industrial waste heat. They need to be protected from contamination which would cause premature wear.
HYDAC supports pioneering large-scale projects, such as “Circulago”. In this project, the small towns of Zug and Baar in Switzerland use water from Lake Zug to generate energy and control the temperature of homes. The aim is to increase the percentage of renewable energy. Optimal temperature transmission and smooth system operation is ensured by providing heat exchangers with optimal protection. This involves four HYDAC automatic back-flushing filters filtering sand and biological material out of the water. With their extensive filter area, they can handle large volumes of water with ease and clean themselves 100% automatically.
Water Treatment is needed EverywhereOur water filters support you with this in industrial applications
No matter whether it's in industry, in municipal waste water treatment plants on ships or in one of the fastest growing areas of food production, aquaculture, with thorough water treatment you can protect important system components such as metering orifices, pumps, mechanical seals and heat exchangers. This means you can save on energy costs, by minimising pressure loss, for example. Our automatic back-flushing filters, screen basket filters and inline filters help to get this done.