Mounting hydrogen tanks securely – with the world's first smart band strap

To achieve the European Green Deal's emission reduction targets, industry and business are increasingly focusing on hydrogen as a climate-neutral energy source. When transporting the volatile fuel, however - in buses, lorries or machines, for example - special requirements must be met in terms of safety and reliability. HYDAC has taken these special circumstances into account with the innovative "HY-ROS H2 Mount Smart" solution - the world's first sensor-based band strap for hydrogen tanks.

Discover our HYDAC mounting solutions for secure hydrogen transport

Would you like to find out more about our innovative mounting solutions for safe hydrogen transport? Arrange a no-obligation consultation appointment with our experts now!

Contact us now!

Secure mounts for breathing hydrogen tanks (type IV) The changing size of hydrogen tanks poses challenges for vehicle manufacturers

Hydrogen tanks (type IV) change their circumference by up to 2.5 per cent during both the refuelling process and emptying process. With conventional solutions that don't compensate for this "breathing", the system's holding force can be impaired.

Reliable tank mount monitoring at every fill level Deviations in the mount's tension state must be detected at an early stage

If significant deviations in the circumference of the hydrogen tank are detected, measures must be taken in good time to ensure that the system's secure hold is not jeopardised. The earlier differences are recognised, the greater the safety for the system and therefore the driver. This is why the reliability of our band straps is carefully validated under laboratory conditions.

Our solution: HY-ROS H2 Mount SmartOur world's first sensor-based band strap for hydrogen tanks enables predictive maintenance

With the HY-ROS H2 Mount Smart, HYDAC is making an innovative contribution to the safety of hydrogen vehicles. This is because the sensor-based band strap enables the tank mount to be reliably monitored in real time. The preventive approach, comparable to a tyre pressure monitoring system, provides continuous data on the condition and integrity of the mounting solution, allowing any deviations to be detected at an early stage and appropriate measures to be initiated.

More information on the HY-ROS H2 Mount Smart band strap

Jochen Caspari, Head of Development at HYDAC Accessories

We validate our HY-ROS band straps with more than 20,000 tank cycles without loss of function. Our mounting solution for hydrogen tanks therefore exceeds both the normal life cycle of a machine and the legal requirements for the approval of tanks of 15,000 cycles.

HYDAC is your partner for secure hydrogen tank mounting Discover the many benefits of the HY-ROS H2 Mount Smart now – the world's first sensor-based band strap to help you mount your hydrogen tanks securely

Our hydrogen tank mount is tried-and-tested

Tried-and-tested hydrogen tank mount

The reliability of our mounting solutions for hydrogen transport has already been confirmed over more than 10 trillion kilometres of travelling.

Our hydrogen tank band straps exceed the legal requirements

Exceeds the legal requirements

Our HY-ROS H2 Mount band straps have been tested beyond the legal requirements for more than 20,000 tank cycles without loss of function.

Our hydrogen band straps enable more efficient maintenance with predictive maintenance

More efficient maintenance with predictive maintenance

Our mounting solution's preventative approach enables early detection and rectification of any deviations that occur.

Downloads

Your expert in hydrogen mounting technology

Contact our team of HYDAC experts and arrange a consultation appointment!

Contact us now

More articles on the topic of mounting technology

Topics & Products
| 3 min

Is all mounting technology created equal? Not always: HYDAC offers more than just first-class quality. We rely on fully automated, in-house production. For us, this means a “Made in Germany” promise. Your advantages are plain to see. We deliver quickly and drive forward custom developments in the shortest possible time frame. With our innovative R&D team, we develop tailor-made solutions which can also be adapted to your individual challenge. Or would you prefer our standard solution optimised for installation? Discover our systems now and put us to the test!