Scrap baling press Optimising scrap baling presses with compact and efficient hydraulic power units

HYDAC – Your partner for tailor-made hydraulic solutions in presses

Optimising scrap baling presses with compact and efficient hydraulic power unitsHYDAC – Your partner for tailor-made hydraulic solutions in presses

Groaning metal and crunching glass: scrap baling presses apply tremendous forces. That’s how the strongest metal scrap turns into a small compact cube. The hydraulic device enables a significant reduction in volume or increase in the density. This results in logistical and economic advantages, especially in terms of transport and further processing. But like every industry, the recycling industry is facing new challenges.

With conventional tank designs, high cylinder speeds and large cylinder diameters lead to traditionally large oil tanks. This doesn't just take up valuable installation space. It also requires many litres of oil, costing you money. The tank optimisation developed by HYDAC remedies this using a flow simulation of the fluids in the tank combined with special patented filters which enable accelerated degassing of the air. This not only reduces the tank size and therefore the installation space. It also saves hydraulic oil. Furthermore, increasing connection and energy costs are leading to the desire to use the most efficient drives possible in order to reduce the drive power and power dissipation.

Reliable, fast and compactHYDAC offers the right hydraulic solution for every baling press

Developing the most compact hydraulic power unit possible – that was our customer’s job for the HYDAC experts. The recycling plant manufacturer focuses on scrap shears and scrap baling presses and produces several new machines per year. They also carry out mechanical and hydraulic service work on existing systems. As part of a job to integrate a new baling press into an existing system, the recycling plant manufacturer asked HYDAC for a total hydraulic solution for their machine.

In close cooperation with the customer, our HYDAC experts defined several goals straight away. Due to the limited spatial conditions, the most compact hydraulic power unit possible was to be developed, saving valuable installation space. As part of this, the oil tank size and the associated size of the drip tray were to be reduced. The main goals were to ensure an energy-efficient hydraulic power unit and a reliable, fast machine with short cycle times. The customer also wanted individual support throughout the entire project phase.

The HYDAC solutionThe tailor-made hydraulic power unit for a 170-tonne scrap baling press

What was particularly important for us when developing the tailor-made solutions? Transparency and communicating as equal partners. It was precisely according to this motto that we defined the dimensions of the hydraulic power unit as well as the necessary technical and hydraulic requirements for the press control in several conversations with our customer.

How we developed the tailor-made solution:

First, we reduced the press oil tank size using our precise flow simulation in combination with our patented AirX filters. This measure doesn't just save installation space. It also aids better air separation and achieves a significant increase in the service life of all hydraulic components. Our custom compact baler control block was equipped with special valve circuitry for the cylinder control. Two axial piston pumps PPV 102-360 with power controllers ensured an efficient reduction in the drive power. As an additional extra, we used our low-noise cooler to take the noise requirements for installation in the industrial hall into consideration.

 

The result

The tailor-made HYDAC solution exceeded our customer’s expectations: by optimising the tank, we reduced the oil tank size by 53% – from 3,200 to 1,500 litres. This allowed the hydraulic power unit to fit in the intended space. Thanks to the compact design, the customer now saves 1,700 litres of hydraulic oil per filling and 5,400 kg of CO2 as a result. In combination with the two power-controlled axial piston pumps, the special valve circuitry in the baler control block achieved a shortened cycle time of 25 seconds instead of 30 seconds. This increased production by 17%. Thanks to the efficient use of the pump flow rate and the motor power over the entire pressure range, the required pump flow amount and therefore the average power consumption were reduced compared to pump combinations with flanged fixed displacement pumps. The nominal power of the motors was reduced from 75 to 55 kW. By replacing the internal gear pumps with power-controlled axial piston pumps, the power losses were greatly reduced. For example, losses from the pumps in circulation amounting to 5.3 kW were avoided, among others. In the future, this will also save 8,960 kWh of energy per year.

What our customer’s case shows:

Our tailor-made solutions increase your efficiency while protecting your budget. Talk to our industry experts now to optimise your system.

Your advantages at a glance

Tailor-made solution

Tailor-made solutions

Our HYDAC specialists develop tailor-made installations for your hydraulic power units as well as other components and solutions.

Increased productivity

Increase your productivity

Significantly increase your performance and save money.

Conservation of resources

Conservation of resources

Whether it's oil, water or energy - our solutions sustainably conserve your resources.

Reduzieren Sie mit Condition Monitoring und Predictive Maintenance Ihren Energieaufwand und sparen Sie so bares Geld.

Energy efficiency

We reduce your power losses – increase your energy efficiency now.

DownloadReference: Optimising scrap baling presses with compact and efficient hydraulic power units

Download reference story in PDF format

We are always happy to give advice!

Contact our HYDAC expert team and arrange your consultation appointment today!

Send an e-mail

Explore more magazine articles

Optimising briquetting presses with compact and efficient hydraulic power units

Customer Success Story
| 3 min

Optimising briquetting presses with compact and efficient hydraulic power units. HYDAC – Your partner for tailor-made hydraulic solutions in presses.